To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
FOR IMMEDIATE RELEASE No. 3164
Will lead to smaller, more efficient power equipment for railcars and electric power systems
TOKYO, January 31, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has developed a 6.5 kV full silicon carbide (SiC) power semiconductor module that is believed to offer the world's highest power density (calculated from rated voltage and current) among power semiconductor modules rated from 1.7 kV to 6.5 kV. The unprecedented power density is made possible by the model's original structure with integrated metal-oxide-semiconductor field-effect transistor (MOSFET) and diode on single chip and its newly developed package. Mitsubishi Electric expects the module to lead to smaller and more energy-efficient power equipment for high-voltage railcars and electric power systems. Going forward, the company will continue to further develop the technology and conduct further reliability tests.
Power density | Power loss | Assumed operating frequency | |
---|---|---|---|
Full-SiC module | 1.8* | 1/3 | 4 |
Conventional silicon IGBT module | 1** | 1 | 1 |
Note: Values normalized to corresponding values of Mitsubishi Electric's conventional silicon IGBT module
*Corresponds to 9.3 kVA/cm3
**Corresponds to 5.1 kVA/cm3
Note that the releases are accurate at the time of publication but may be subject to change without notice.