News Releases

Australia’s Smallest Air Conditioning Unit Is Here
Perfect For Home Offices & Bedrooms

SYDNEY, Australia, 23 March 2021: Mitsubishi Electric Australia has announced the launch of the MSZ-AP 15/20 Mini Series, the newest air conditioning system, designed for year round comfort in small spaces.

The MSZ-AP 15/20 Mini Series is a sleek and compact wall-mounted split-system air conditioning unit and has the smallest indoor unit dimensions in the Australian market at just 250 mm (h) x 760 mm (w). This size makes it perfect for installation above a door or window frame and the ideal solution for a bedroom or home office.

Although the MSZ-AP15/20 was designed with smaller rooms in mind, the cooling output isn’t compromised operating at 1.5 / 2.0 kw and delivers an effective cooling solution in a discrete unit.

Atesh Mani, National Product Manager at Mitsubishi Electric Australia, explained that the model’s dimensions does not mean it lacks on performance.

‘Quite often you find Australians have units that are too large for their needs in their bedroom or study, which is poor for system efficiency. Despite its compact design, the MSZ-AP Mini Series, provides effective and targeted cooling in smaller rooms. This is ideal for when you only need to cool one room at a time and to ensure year round comfort when you’re trying to sleep or work from home,’ Atesh said.

‘The compact dimensions allow the indoor unit to be installed centred in the room, above a door or window frames, instead of off to one side, which is the case for larger units. This flexibility in installation position lends itself to more aesthetically pleasing room designs,’ Atesh continued.

Another key benefit of the MSZ-AP Mini series is that it requires less cleaning required due to Dual Barrier Coating. This coating reduces dust and greasy dirt from collecting on its inner surfaces, ensuring that those who instal it in their home will have a clean air conditioner year-round.

The MSZ-AP Mini Series can be controlled via Wi-Fi Control*1. This innovative technology connects the Mitsubishi Electric air conditioner to the user’s smartphone, tablet or online account, giving them the freedom to fully control each unit on-the-go via an internet connection, perfect for when users want their room at the perfect temperature when they arrive home.

  1. *1 Optional Wi-Fi adapter required per unit.
    Requires an internet connection and the App downloaded on your smartphone or tablet with the latest operation system available.

Models:

  • MSZ-AP15VGD-A 1.5 kW cooling / 1.7 kW heating – P.O.A. Available for multi split connection only.
  • MSZ-AP20VGD-A 2.0 kW cooling / 2.5 kW heating – RRP$1499

For further information on the Mitsubishi Electric MSZ-AP Mini Series, visit https://www.mitsubishielectric.com.au/product/msz-ap-mini/

Mitsubishi Electric, works for me.
For more information, visit us at www.mitsubishielectric.com.au

For more information contact:
Kristina Gatsos , Thrive PR
Email: (mail link)kristina.gatsos@thrivepr.com.au


Note

Note that the press releases are accurate at the time of publication but may be subject to change without notice.