Products & Solutions

Factory Automation Systems

Offering a vast range of automation and processing technologies, including controllers, drive products, power distribution and control products, electrical discharge machines, electron beam machines, laser processing machines, computerised numerical controllers and industrial robots, Mitsubishi Electric helps bring higher productivity—and quality—to the factory floor. In addition, our extensive service networks around the globe provide direct communication and comprehensive support to customers.

Product Line-up

Controllers

Programmable Controllers—MELSEC

Programmable Controllers—MELSEC

The Q Series PLCs are equipped with a multiple CPU function that allows multiple CPUs to be mounted simultaneously. This capability allows for system configurations that match the scale and objectives of the production site.

(open new window)Learn more

Simple Application Controllers

Simple Application Controllers

The FX series can be easily used in all places where control is needed for the home, office or factory.

(open new window)Learn more

Motion Controllers

Motion Controllers

Controllers that provide highly accurate positioning control. The servo is controlled by way of a high-speed servo network SSCNET, making complex synchronous control easy.

(open new window)Learn more

Computerised Numerical Controllers — CNCs

Computerised Numerical Controllers — CNCs

CNCs are the core of machine tool systems, which are commonly called the "mother machine" in the manufacturing industry. Mitsubishi Electric's CNCs are equipped with the latest CPU and high-speed optic servo network, to provide high-speed and high-precision machining. They contribute to increasing productivity in the automotive and IT industries, as well as in a wide variety of other industries.

(open new window)Learn more

Data Logging Analyser — MELQIC

Data Logging Analyser — MELQIC

The MELQIC data logging analyser is a powerful device that inspects products and records data. An optimum inspection programme can dramatically shorten the tact time of the inspection process. MELQIC can also respond flexibly to line modifications.

(open new window)Learn more

Drive Products

AC Servos — MELSERVO

AC Servos — MELSERVO

MELSERVO systems combine a servo motor and amp, and are ideal for controlling the moving parts of various machines and equipment (speed, torque, alignment, locus etc.). They contribute to the development of competitive devices, as a driving source for industrial machines.

(open new window)Learn more

Inverters — FREQROL

Inverters — FREQROL

The FREQROL Series general-purpose inverters allows changes to be made to the speed of three-phase induction motors, freely and easily. An extensive line-up provides optimum control and energy conservation in a wide range of machines.

(open new window)Learn more

Visualisation

Human-Machine Interfaces (HMIs) — GOT

Human-Machine Interfaces (HMIs) — GOT

Human-Machine Interfaces (HMIs) — GOT The GOT Series HMIs have been designed to deliver maximum usability. They contribute to our customers' needs to improve efficiency, increase productivity and create added-value, by allowing them to monitor information from PLCs, CNCs and other FA products, and modify various data, through the HMIs.

(open new window)Learn more

SCADA MC Work

SCADA MC Work

MC Works64 can monitor plant-wide operation and support efficient plant operations. It is an integral software providing a variety of functions and refined user interfaces suitable for social infrastructure fields.

(open new window)Learn more

Industrial Robots

Industrial Robots — MELFA

Industrial Robots — MELFA

Smaller, lighter and faster robots that are capable of managing heavier loads, both in terms of weight and functionality. Advanced developments at Mitsubishi Electric include the addition of a dedicated motor and controller fitted with a T64-bit RICS chip set. Models in the line-up are now equipped with a collision detection function and are being used to automate a growing number of production facilities where they contribute to added-value production.

(open new window)Learn more

Low-voltage Power Distribution Products

Low-voltage Circuit Breakers

Low-voltage Circuit Breakers

Mitsubishi Electric's no-fuse breakers and earth-leakage circuit breakers comply with overseas standards, including European and Chinese standards. A wide array of products, including the new eco-friendly WS-V Series, responds to various energy-saving and space-saving needs of our clients.

(open new window)Learn more

Contactors and Motor Starters

Contactors and Motor Starters

Electromagnetic contactors are used to control (run/stop) machine tools, air-conditioners, lighting equipment etc. Mitsubishi Electric offers a wide line-up of contactors to satisfy various control applications.

(open new window)Learn more

Power Monitoring Products

Power Management Meters

Power Management Meters

Mitsubishi Electric's wide array of measuring devices suits various applications, such as quantifying, measuring, displaying, recording, and monitoring electric power, current and voltage in plants and buildings.

(open new window)Learn more

Energy Saving Supporting Devices

Energy Saving Supporting Devices

Support energy saving activities by "visualising" solution with Energy Saving Supporting Devices.

(open new window)Learn more

Medium-voltage Power Distribution Products

High-voltage Alternating Current Circuit Breakers and High-voltage Alternating Current Contactors

High-voltage Alternating Current Circuit Breakers and High-voltage Alternating Current Contactors

Meet the needs for environment conservation, safety, electric power saving and international standards.

(open new window)Learn more

Protection Relays

Protection Relays

Indispensable protection relays to accommodate the improved reliability of power distribution systems. Offering the appropriate products for various industrial areas.

(open new window)Learn more

Processing Machines

Laser Processing Machines

Laser Processing Machines

Mitsubishi Electric has a vast line-up of laser processing machines, from 2-dimensional processing units to 3-dimensional, hole-drilling and large-workpiece machines. All provide unprecedented levels of accuracy and speed for processing various materials of virtually any shape or size. A full-service system awaits, complete with product consultation, product training, custom programming software development, after-sales service and more. A leading player in the global market, these products offer shorter processing times, impressive energy savings and astounding surface finish quality.

  • 2D Laser Processing Machines
  • 3D Laser Processing Machines
  • Laser Drilling Machines
(open new window)Learn more

Electrical Discharge Machines — EDM

Electrical Discharge Machines — EDM

Mitsubishi Electric's state-of-the-art EDMs are used in the manufacturing processes of medical equipment, semiconductors, electronic devices and more. A plethora of innovative technologies are incorporated to ensure highly precise, fast processing that not only expands the range of production applications, but also contributes to the manufacturing of reliable, high-quality products that provide optimum performance.

  • Die-Sinking EDM
  • Wire-Cut EDM
  • Fine-hole Drilling EDM
  • Micro Spark Coating — MS Coating
(open new window)Learn more

Electron Beam Machines — EBM

Electron Beam Machines — EBM

Used in a variety of processes from precision welding, alloying, and surface modification to soldering, Mitsubishi Electric's electron beam machines present new, high value-added applications to various industrial fields, and the automotive industry in particular. The applications of electron beam machines are also expanding to advanced segments of the IT industry, where they are employed in the micro welding of electronic device components.

(open new window)Learn more

For more information