To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
FOR IMMEDIATE RELEASE No. 3066
AR smart glasses help to reduce workload and confirm data accuracy
TOKYO, November 7, 2016 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it has developed a maintenance-support technology using augmented reality (AR) based on a three-dimensional model that enables a technician wearing smart glasses to confirm the order of the inspection on an AR display and then enter the results by voice. The technology helps reduce workload and avoid entry errors because information can be entered by voice, even in noisy environments. The system is expected to be used for a variety of maintenance work, such as inspections of water-treatment plants and building electrical systems.
Mitsubishi Electric's new AR systems realizes highly intuitive inspections
New technology | Conventional technology | |
---|---|---|
Function | AR display based on three-dimensional model | Two-dimensional AR display |
Voice recognition using deep learning | Voice recognition using simple statistical model (Hidden Markov Model) |
|
Performance | Object positioning with max. 1.2 cm error at 60 cm | Object positioning with max. 4.0 cm error at 60 cm |
95 % accuracy at max. 85dbA | 90 % accuracy at max. 85dbA |
Note that the releases are accurate at the time of publication but may be subject to change without notice.