To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
FOR IMMEDIATE RELEASE No. 3067
TOKYO, November 10, 2016 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that its new S-series of escalators, which offer enhanced passenger safety and high-level energy conservation, will launch on November 14. Annual sales of 1,000 units are targeted outside of Japan.
Mitsubishi S-series Escalators
Product name | Type* | Rated speed | Price | Launch | Targeted sales |
---|---|---|---|---|---|
S-series Escalator | Type S1000 Type S800 Type S600 |
30 meters per minute | By quote | November 14 | 1,000 units per annum |
*Passengers per step - S1000 (step width: 1,000 mm): 2 passengers; Type S800 (800 mm) and Type S600 (600 mm): 1 passenger
Note that the releases are accurate at the time of publication but may be subject to change without notice.