To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
FOR IMMEDIATE RELEASE No. 3103
TOKYO, May 8, 2017 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the launch of a 19.0-inch SXGA color TFT-LCD module, which is equipped with a projected capacitive touch panel utilizing a cover glass of up to 5 millimeters in thickness. Sample sales will begin on June 30 via Mitsubishi Electric offices worldwide. The new module will be presented at the 20th Embedded Systems Expo (ESEC Spring) at the Tokyo Big Sight exhibition complex from May 10 to 12.
The new module will meet increasing industrial demands for extra-thick or glove-operable cover glass. It also enables accurate, multi-touch sensing even when the screen is wet. The combination of these cutting-edge touch capabilities and Mitsubishi Electric's proven TFT-LCD technologies will support diverse applications and installations.
Product | Model | Display Size | Resolution | LED Driver | Shipment |
---|---|---|---|---|---|
TFT-LCD Module with Projected Capacitive touch panel |
AA190EB02-PCAP | 19.0-inch | SXGA | Provided | June 30, 2017 |
Note that the releases are accurate at the time of publication but may be subject to change without notice.