To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
FOR IMMEDIATE RELEASE No. 3208
Ideal for versatile outdoor measuring instruments and industrial devices
TOKYO, August 22, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today the coming launch of a new 7.0-inch WXGA TFT-LCD module for industrial applications including outdoor measuring instruments, devices and more. The module will offer an unprecedented combination of high-resolution WXGA (1,280 x 768 dots), super-wide 176-degree horizontal/vertical viewing angles, high brightness of 1,000 cd/m2 , a high contrast ratio of 1000:1, a versatile operating temperature range of -40 to 80 degrees Celsius, and high vibration resistance. Sample sales will begin September 20 through Mitsubishi Electric offices worldwide.
The new TFT-LCD module will satisfy increasing market demands for versatile applications and installations requiring features such as high resolution, wide viewing angles, high brightness and high resistance to vibrations and extreme temperatures.
Mitsubishi Electric now offers 34 TFT-LCD modules with super-wide viewing angles.
Product | Model | LED driver | Sample Shipments |
---|---|---|---|
7.0-inch WXGA TFT-LCD Module | AA070TA01 | Implemented | September 20, 2018 |
AA070TA11 | ─ |
Note that the releases are accurate at the time of publication but may be subject to change without notice.