To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
FOR IMMEDIATE RELEASE No. 3235
Unprecedented 3.0W pulse-light output power will lead to extra-bright and miniaturized projectors
TOKYO, December 19, 2018 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will launch the ML562G86 pulse laser diode (LD) for projectors, featuring a vibrant 638-nanometer (nm) red light, world-record output power of 3.0W under pulse operation and mean time to failure1 (MTTF) of over 20,000 hours, on April 1, 2019. The ML562G86's high output power and wide operating temperature range will contribute to enhanced projector luminance and miniaturization. Sample sales will begin on January 11, 2019.
1 Standard evaluation of reliability
Note that the releases are accurate at the time of publication but may be subject to change without notice.