To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
News Releases
FOR IMMEDIATE RELEASE No. 3378
TOKYO, October 1, 2020 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that construction of its SUSTIE net zero-energy building (ZEB) test facility located on the premises of the company's Information Technology R&D Center in Kamakura, Japan, will be completed on October 14. In line with the company's support for Sustainable Development Goals (SDGs), the facility will facilitate accelerated development and testing of increasingly common ZEB-compliant energy -conservation technologies as well as contribute to the realization of more comfortable and energy-efficient indoor environments.
SUSTIE ZEB Test Facility
SUSTIE's logo
ZEBs are buildings that offer comfortable indoor environments while maintaining annual primary energy consumption at or near zero through means such as thermal insulation, solar radiation shielding, natural energy usage and facility efficiency. As a ZEB Planner1, Mitsubishi Electric is contributing to the adoption of ZEBs by providing planning and business support to help companies develop their own ZEBs. The SUSTIE test facility will be used for wide-ranging demonstrations and verifications to accelerate the further development of ZEB technologies. Research and development will be advanced in accordance with Mitsubishi Electric's ZEB+®2 philosophy. The concept for SUSTIE was developed in collaboration with Professor Shin-ichi Tanabe of Faculty of Science and Engineering at Waseda University in Tokyo; the SUSTIE was designed and construction supervised by Mitsubishi Jisho Sekkei. The name "SUSTIE" combines the words "sustainability" and "energy" to express the idea of an office for researching and demonstrating energy conservation and comfort.
Location | 5-1-1 Ofuna, Kamakura, Kanagawa Prefecture, Japan (premises of Information Technology R&D Center, Mitsubishi Electric Corporation) |
Area/construction | Building: 1,950 m2; Total floor space: 6,460 m2; 4-story steel-framed |
Investment | 4 billion yen (38 million USD) including 1.6 billion yen (15.2 million USD) for demonstration equipment |
Launch | Full-scale startup in January 2021 |
Energy performance | World-leading BEI3 primary energy consumption evaluation index of —0.06 (or 0.41 excluding solar power- energy generation) as midsized office building of at least 6,000 m2 |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.