To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
News Releases
FOR IMMEDIATE RELEASE No. 3397
TOKYO, February 18, 2021 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today that two new 13.75-14.5 GHz (Ku-band) 30W (45.3dBm) gallium-nitride high-electron-mobility transistors (GaN HEMTs) will be added to the company's GaN HEMT lineup for satellite-communication (SATCOM) earth stations. The two products, one for multi-carrier1 communication and the other for single-carrier2 communication, will support increased data-transmission capacity and smaller earth stations. Sales will begin on March 15.
GaN HEMTs for Ku-band SATCOM earth stations
Single-carrier 30W MGFK45G3745 (left) and multi-carrier 30W MGFK45G3745A (right)
Ku-band satellite systems are increasingly being deployed for emergency communication during natural disasters and for satellite news gathering (SNG) by TV broadcasters in remote areas where cable networks do not exist. Meanwhile, in addition to the growing use of conventional single-carrier communication, multi-carrier communication is increasingly needed for fast, high-volume communication and to support the downsizing of mobile stations for purposes such as SNG. So far, Mitsubishi Electric has introduced five GaN HEMTs for multi-carrier and single-carrier SATCOM earth stations. The two new 30W GaN HEMTs will enable more flexible amplifier designs, including for rated power levels and the use of GaN drivers. They also will support the downsizing of earth stations as well as faster, larger-capacity satellite communication.
Product | Application | Model | Overview | Release | ||
---|---|---|---|---|---|---|
Frequency | Saturated output power |
Application | ||||
Ku-band GaN- HEMTs |
SATCOM earth stations |
MGFK45G3745A | 13.75-14.5 GHz |
45.3dBm (30W) |
Multi-carrier | Mar. 15, 2021 |
MGFK45G3745 | 45.3dBm (30W) |
Single-carrier |
The MGFK45G3745A for multi-carrier communications delivers low IMD33 with wide offset frequencies4 of up to 400MHz for large-capacity, high-speed satellite communication.
Multi-carrier communication (new model in bold)
Model | MGFK45G3745A | MGFK48G3745A | MGFK50G3745A |
Frequency | 13.75GHz-14.5GHz | ||
Saturated output power |
45.3dBm (30W) |
48.3dBm (70W) |
50.0dBm (100W) |
Linear gain | 9.5dB | 11dB | 10dB |
Offset frequency @IMD3 = -25dBc |
Up to 400MHz | Up to 400MHz | Up to 200MHz |
Single-carrier communication (new model in bold)
Model | MGFK45G3745 | MGFK48G3745 | MGFK50G3745 | MGFG5H1503 |
Frequency | 13.75GHz-14.5GHz | |||
Saturated output power |
45.3dBm (30W) |
48.3dBm (70W) |
50.0dBm (100W) |
43.0dBm (20W) |
Linear gain | 9.5dB | 12dB | 10dB | 24dB |
Offset frequency @IMD3 = -25dBc |
Up to 5MHz | Up to 5MHz | Up to 5MHz | Up to 5MHz |
Note that the press releases are accurate at the time of publication but may be subject to change without notice.