News Releases
Mitsubishi Electric Achieves World's First Wideband Operation of 4G, 5G and Beyond 5G/6G Systems with Single GaN Power AmplifierWill help to realize radio-unit sharing and power-efficient base stations
FOR IMMEDIATE RELEASE No. 3611

Image of the base-stations with before/after amplifiers
TOKYO, June 8, 2023 - Mitsubishi Electric Corporation (TOKYO: 6503) announced today it has developed what is believed to be the world's first* gallium nitride (GaN) power amplifier that achieves a frequency range of 3,400MHz using a single power amplifier, which the company has demonstrated can be used for 4G, 5G and Beyond 5G/6G communication systems operating at different frequencies in a single base station. The amplifier is expected to enable the radio unit (transceiver) to be shared for different communication systems and lead to more power-efficient base stations. Technical details will be presented at the IEEE International Microwave Symposium 2023 this month.
- * According to Mitsubishi Electric research as of June 8, 2023
Note
Note that the press releases are accurate at the time of publication but may be subject to change without notice.