To make our site as user friendly as possible we use cookies. Please confirm that you agree to our use of cookies by clicking Yes.
News Releases
SYDNEY, Australia, 1 April 2025 – Mitsubishi Electric, one of the world’s leading names in air conditioning solutions, is excited to announce that its MSZ-AP Series, MSZ-EF Series, and MFZ-KW Series will now have built-in Wi-Fi connectivity. This welcome feature offers Australians unparalleled convenience, allowing users to control their comfort anywhere, anytime.
The integration of Wi-Fi into Mitsubishi Electric air conditioning units enables users to remotely adjust settings, including temperature, mode, and fan speed, through the app, which is compatible with both iOS and Android devices.
This latest technology advancement from Mitsubishi Electric will roll out across three of its popular air conditioner series:
Capacity Range: 2.0/2.5/3.5/4.2/5.0/6.0/7.1/7.8kW
The MSZ-AP Series is engineered for high performance and lower operating noise levels and has a streamlined design to blend in with décor. Features include:
*Built-In Wi-Fi not available with the MSZ-AP20VGD2
Capacity Range: 2.5/3.5/4.2/5.0 kW
The streamlined wall-mounted indoor units have contemporary, clean lines, expressing sophistication and quality, in a modern design. Features include:
Capacity Range: 2.5/3.5/4.2/5.0/6.0kW
These floor consoles are a great renovation option with their slimline design, fitting neatly into cavities of renovated fireplaces or heaters. Features include:
With the introduction of built-in Wi-Fi to these products, Mitsubishi Electric continues to lead the way in delivering innovative, energy-efficient, and user-friendly air conditioning solutions for Australian homes and businesses.
"Smart technology is now an essential part of modern living, and Mitsubishi Electric is proud to offer cutting-edge solutions that blend innovation with everyday convenience," said Atesh Mani, National Product Manager at Mitsubishi Electric Australia.
"With this latest development, our customers can experience greater flexibility, energy savings, and most importantly, comfort. Whether they’re coming home to a cool environment or adjusting the settings while they’re away, our air conditioners are now more connected than ever before."
For more information, please visit www.mitsubishielectric.com.au
A Life More Electric
Spokesperson:
Atesh Mani, National Product Manager at Mitsubishi Electric Australia
For more information contact:
Mitsubishi Electric Australia Pty. Ltd.
Email:communications@meaust.meap.com
Note that the press releases are accurate at the time of publication but may be subject to change without notice.